Compact 800 RunTime FB - Version 1.1 (.zip)
App id
20194747
File extension
.zip
File name
5508_Runtime-Hour-functionblock-for-Compact-control-builder_1-1.zip
Type
App
Version
1.1
File size
1.9 MB
In addition to previous version, now FB in this version can count valve/motor/pumps number of start/stop or open/close count to help maintenance staff to service equipment. As well can show last start date and time and user can set limit of no. of start/stop to get alarm when limit is reached.
Version
Description
1.1 by Sumit Gargav
In addition to previous version, now FB in this version can count valve/motor/pumps number of start/stop or open/close count to help maintenance staff to service equipment. As well can show last start date and time and user can set limit of no. of start/stop to get alarm when limit is reached.
UFB function description :
At the beginning T1, T2,T3, T4 values are zero.
Once block gets run feedback at Run_In pin, it starts calculating current time(T1), cumulative time(T3), total time(T4).(FIG-2)
In between if run indication fails(or equipment not running) than current time(T1) get stored as previous time(T2) & current time(T1) will start with new/fresh time count. But cumulative time(T3) and Totaltime (T4) get calculated continuously.
Total time(T4) never get reset from faceplate. This time gives total runtime value.
If operator will press RESET in between operation than T1,T2, T3 will reset to zero & again start with a new count.
Contributed by Govindaraj and Ramayak,
This App is Free for Limited period, Enjoy using it....
At the beginning T1, T2,T3, T4 values are zero.
Once block gets run feedback at Run_In pin, it starts calculating current time(T1), cumulative time(T3), total time(T4).(FIG-2)
In between if run indication fails(or equipment not running) than current time(T1) get stored as previous time(T2) & current time(T1) will start with new/fresh time count. But cumulative time(T3) and Totaltime (T4) get calculated continuously.
Total time(T4) never get reset from faceplate. This time gives total runtime value.
If operator will press RESET in between operation than T1,T2, T3 will reset to zero & again start with a new count.
Contributed by Govindaraj and Ramayak,
This App is Free for Limited period, Enjoy using it....
You must be logged in and have downloaded this app in order to post a review or rating. Login
Posted by
on
Apr 12, 2018 at 03:52 AM
Posted by
on
Apr 12, 2018 at 03:52 AM
Posted by
on
Jan 30, 2016 at 06:16 AM
Posted by
on
Sep 10, 2015 at 05:32 AM
Posted by
on
Aug 04, 2015 at 04:35 AM