Softcontroller Administrator - Version 1.2 (.zip)
App id
20194743
File extension
.zip
File name
4346_SoftController-Pro_1-2.zip
Type
App
Version
1.2
File size
199 KB
In this version changed App name to Softcontroller Pro and icon
bug fix as well.
The software is extremely simple, no installation is required. only one exe file Functions are also simple: create SC, remove SC and start/stop SC support 4.1 to 5.1 FP4 support 32, 64bit windows support MMS communication between SC support HI or normal SC support MMS ID from 3-50 ( didn't test so many SC) Setting of Hi or normal will write to register table ( make sure your Anti-Virus doesn't block it) Note1, you must install official soft controller first. Note2, MMS ID number 22 is reserved for AC800M OPC software. Note3, 4.1 system may require Microsoft .net frame 3.5 Last, use at your own risk.
bug fix as well.
The software is extremely simple, no installation is required. only one exe file Functions are also simple: create SC, remove SC and start/stop SC support 4.1 to 5.1 FP4 support 32, 64bit windows support MMS communication between SC support HI or normal SC support MMS ID from 3-50 ( didn't test so many SC) Setting of Hi or normal will write to register table ( make sure your Anti-Virus doesn't block it) Note1, you must install official soft controller first. Note2, MMS ID number 22 is reserved for AC800M OPC software. Note3, 4.1 system may require Microsoft .net frame 3.5 Last, use at your own risk.
Version
Description
1: change to single instance application.
-so that you won't start duplicated Soft controller Pro by mistake.
2: double click notify icon to call back main instance.
3: support SV6.0 soft controller
-although multiple- sc is finally supported by SV6.0 official
-find more in release notes
-so that you won't start duplicated Soft controller Pro by mistake.
2: double click notify icon to call back main instance.
3: support SV6.0 soft controller
-although multiple- sc is finally supported by SV6.0 official
-find more in release notes
1.2 by Awesomedays
In this version changed App name to Softcontroller Pro and icon
bug fix as well.
The software is extremely simple, no installation is required. only one exe file Functions are also simple: create SC, remove SC and start/stop SC support 4.1 to 5.1 FP4 support 32, 64bit windows support MMS communication between SC support HI or normal SC support MMS ID from 3-50 ( didn't test so many SC) Setting of Hi or normal will write to register table ( make sure your Anti-Virus doesn't block it) Note1, you must install official soft controller first. Note2, MMS ID number 22 is reserved for AC800M OPC software. Note3, 4.1 system may require Microsoft .net frame 3.5 Last, use at your own risk.
bug fix as well.
The software is extremely simple, no installation is required. only one exe file Functions are also simple: create SC, remove SC and start/stop SC support 4.1 to 5.1 FP4 support 32, 64bit windows support MMS communication between SC support HI or normal SC support MMS ID from 3-50 ( didn't test so many SC) Setting of Hi or normal will write to register table ( make sure your Anti-Virus doesn't block it) Note1, you must install official soft controller first. Note2, MMS ID number 22 is reserved for AC800M OPC software. Note3, 4.1 system may require Microsoft .net frame 3.5 Last, use at your own risk.
nothing
The software is extremely simple, no installation is required. only one exe file
Functions are also simple: create SC, remove SC and start/stop SC
support 4.1 to 5.1 FP4
support 32, 64bit windows
support MMS communication between SC
support HI or normal SC
support MMS ID from 3-50 ( didn't test so many SC)
Setting of Hi or normal will write to register table ( make sure your Anti-Virus doesn't block it)
Note1, you must install official soft controller first.
Note2, MMS ID number 22 is reserved for AC800M OPC software.
Note3, 4.1 system may require Microsoft .net frame 3.5
Last, use at your own risk.
Functions are also simple: create SC, remove SC and start/stop SC
support 4.1 to 5.1 FP4
support 32, 64bit windows
support MMS communication between SC
support HI or normal SC
support MMS ID from 3-50 ( didn't test so many SC)
Setting of Hi or normal will write to register table ( make sure your Anti-Virus doesn't block it)
Note1, you must install official soft controller first.
Note2, MMS ID number 22 is reserved for AC800M OPC software.
Note3, 4.1 system may require Microsoft .net frame 3.5
Last, use at your own risk.
You must be logged in and have downloaded this app in order to post a review or rating. Login
Posted by
on
Apr 12, 2018 at 03:48 AM
Posted by
on
Apr 12, 2018 at 03:48 AM
Really Useful App...
Posted by on May 16, 2017 at 12:32 AMAn extremely useful App.
Posted by on Aug 05, 2016 at 04:45 AMGood App for Development and Testing.
Posted by on Jul 14, 2016 at 09:46 PMGreat App
Posted by on Mar 05, 2015 at 07:21 AMNice App!
Posted by on Mar 02, 2015 at 09:13 PMGreat app ! It would be ideal being able to change path for SCs. Thanks anyway !
Posted by on Feb 13, 2015 at 03:17 PM
Posted by
on
Feb 09, 2015 at 04:20 AM
It would be nice to be able to set up the SoftControllers on a demo/test system using the same IP adresses as the real controllers on a live system
Posted by on Nov 18, 2014 at 12:38 AMPlease make path-settings working
Posted by on Nov 01, 2014 at 11:09 PM
Posted by
on
Nov 01, 2014 at 08:47 AM
Posted by
on
Nov 01, 2014 at 08:46 AM
Posted by
on
Nov 01, 2014 at 08:46 AM
Posted by
on
Oct 31, 2014 at 02:48 AM