Softcontroller Administrator - Version 1.7 (.zip)
App id
20194743
File extension
.zip
File name
4346_SoftController-Pro_1-7.zip
Type
App
Version
1.7
File size
130 KB
1: change to single instance application.
-so that you won't start duplicated Soft controller Pro by mistake.
2: double click notify icon to call back main instance.
3: support SV6.0 soft controller
-although multiple- sc is finally supported by SV6.0 official
-find more in release notes
-so that you won't start duplicated Soft controller Pro by mistake.
2: double click notify icon to call back main instance.
3: support SV6.0 soft controller
-although multiple- sc is finally supported by SV6.0 official
-find more in release notes
Version
Description
1.7 by Awesomedays
1: change to single instance application.
-so that you won't start duplicated Soft controller Pro by mistake.
2: double click notify icon to call back main instance.
3: support SV6.0 soft controller
-although multiple- sc is finally supported by SV6.0 official
-find more in release notes
-so that you won't start duplicated Soft controller Pro by mistake.
2: double click notify icon to call back main instance.
3: support SV6.0 soft controller
-although multiple- sc is finally supported by SV6.0 official
-find more in release notes
In this version changed App name to Softcontroller Pro and icon
bug fix as well.
The software is extremely simple, no installation is required. only one exe file Functions are also simple: create SC, remove SC and start/stop SC support 4.1 to 5.1 FP4 support 32, 64bit windows support MMS communication between SC support HI or normal SC support MMS ID from 3-50 ( didn't test so many SC) Setting of Hi or normal will write to register table ( make sure your Anti-Virus doesn't block it) Note1, you must install official soft controller first. Note2, MMS ID number 22 is reserved for AC800M OPC software. Note3, 4.1 system may require Microsoft .net frame 3.5 Last, use at your own risk.
bug fix as well.
The software is extremely simple, no installation is required. only one exe file Functions are also simple: create SC, remove SC and start/stop SC support 4.1 to 5.1 FP4 support 32, 64bit windows support MMS communication between SC support HI or normal SC support MMS ID from 3-50 ( didn't test so many SC) Setting of Hi or normal will write to register table ( make sure your Anti-Virus doesn't block it) Note1, you must install official soft controller first. Note2, MMS ID number 22 is reserved for AC800M OPC software. Note3, 4.1 system may require Microsoft .net frame 3.5 Last, use at your own risk.
nothing
The software is extremely simple, no installation is required. only one exe file
Functions are also simple: create SC, remove SC and start/stop SC
support 4.1 to 5.1 FP4
support 32, 64bit windows
support MMS communication between SC
support HI or normal SC
support MMS ID from 3-50 ( didn't test so many SC)
Setting of Hi or normal will write to register table ( make sure your Anti-Virus doesn't block it)
Note1, you must install official soft controller first.
Note2, MMS ID number 22 is reserved for AC800M OPC software.
Note3, 4.1 system may require Microsoft .net frame 3.5
Last, use at your own risk.
Functions are also simple: create SC, remove SC and start/stop SC
support 4.1 to 5.1 FP4
support 32, 64bit windows
support MMS communication between SC
support HI or normal SC
support MMS ID from 3-50 ( didn't test so many SC)
Setting of Hi or normal will write to register table ( make sure your Anti-Virus doesn't block it)
Note1, you must install official soft controller first.
Note2, MMS ID number 22 is reserved for AC800M OPC software.
Note3, 4.1 system may require Microsoft .net frame 3.5
Last, use at your own risk.
You must be logged in and have downloaded this app in order to post a review or rating. Login
Posted by
on
Aug 01, 2018 at 03:43 AM
by admin Rank: 44 on Mar 09, 2015 at 01:34 AM
Not run with softcontroller 5.1.1, have a error "Couldn't read Heapsize from registry.I'm using Compact Control Builder AC 800M version 5.1.1
Posted 38 minutes ago by minoan
by minoan Rank: 4116 on Mar 18, 2015 at 08:44 AM
Thanks, i just only run one soft controller 5.1.1, i can't run two or more soft controllers together.
by Awesomedays Rank: 151 on Mar 15, 2015 at 06:05 PM
this is so call default instance ....lol
https://data2.answerbase.com/ABB/forum-controlsystems.abb.com/UserFiles/Answers201503/answerImage533212-15090414.jpg
by minoan Rank: 4116 on Mar 14, 2015 at 09:10 AM
how to run the soft controller with default instance? Pls.
by Awesomedays Rank: 151 on Mar 09, 2015 at 02:27 AM
can you run the soft controller with default instance ?