Bulk SPL template for bulk configuration of Sequence logic - Version 1.0 (.zip)
App id
20194725
File extension
.zip
File name
985_Bulk_SPL-Template_1-0.zip
Type
App
Version
1.0
File size
19 KB
This is a new template introduced in System 800xA Engineering Studio SV 5.1 Feature Pack3. It is developed to reduce the engineering efforts while configuring big sequence logic. Normally configuring a big sequence is a time consuming process, engineering efforts can be significantly reduced using this template.
Template can be used for Offline engineering as well which means that sequence configuration can be done on a machine with/without 800xA system. Once the configuration is done, logic can be transformed to 800xA system.
Template supports the following sequences:
- Sequence2D: Sequence2D is specific to Function Designer created applications.
- Sequence: This type of sequence can be created using Function Designer as well in Control Builder M.
Attachment consists only a sample of the template. there are some pre-requisites and defined workflows to use it. Refer '3BDS011223-510, Section 4 Bulk SPL'.
Template can be used for Offline engineering as well which means that sequence configuration can be done on a machine with/without 800xA system. Once the configuration is done, logic can be transformed to 800xA system.
Template supports the following sequences:
- Sequence2D: Sequence2D is specific to Function Designer created applications.
- Sequence: This type of sequence can be created using Function Designer as well in Control Builder M.
Attachment consists only a sample of the template. there are some pre-requisites and defined workflows to use it. Refer '3BDS011223-510, Section 4 Bulk SPL'.
Version
Description
1.0 by amit.sisodiya
This is a new template introduced in System 800xA Engineering Studio SV 5.1 Feature Pack3. It is developed to reduce the engineering efforts while configuring big sequence logic. Normally configuring a big sequence is a time consuming process, engineering efforts can be significantly reduced using this template.
Template can be used for Offline engineering as well which means that sequence configuration can be done on a machine with/without 800xA system. Once the configuration is done, logic can be transformed to 800xA system.
Template supports the following sequences:
- Sequence2D: Sequence2D is specific to Function Designer created applications.
- Sequence: This type of sequence can be created using Function Designer as well in Control Builder M.
Attachment consists only a sample of the template. there are some pre-requisites and defined workflows to use it. Refer '3BDS011223-510, Section 4 Bulk SPL'.
Template can be used for Offline engineering as well which means that sequence configuration can be done on a machine with/without 800xA system. Once the configuration is done, logic can be transformed to 800xA system.
Template supports the following sequences:
- Sequence2D: Sequence2D is specific to Function Designer created applications.
- Sequence: This type of sequence can be created using Function Designer as well in Control Builder M.
Attachment consists only a sample of the template. there are some pre-requisites and defined workflows to use it. Refer '3BDS011223-510, Section 4 Bulk SPL'.
You must be logged in and have downloaded this app in order to post a review or rating. Login
Posted by
on
Apr 11, 2018 at 09:45 AM
Good template to start with but UI takes some time to understand and get used to.
Posted by on May 14, 2014 at 12:27 AM
Posted by
on
May 09, 2014 at 11:00 PM