Hourly timer function block freelance - Version 1.0 (.zip)
App id
20194664
File extension
.zip
File name
287_Hourly-timer-function-block-freelance_1-0.zip
Type
App
Version
1.0
File size
154 KB
The block is used for running a timer of preset time during each hour of a day.The block uses the controller time as an input for date and time.The input pins H01, H02…., H24 are for running the timer in a particular hour.The out will be high for preset duration of the timer.The Timer can also be started from the faceplate. The buttons on the faceplate are for running the timer during each hour.Duration, Running current hour and Elapsed time of the timer is shown on the faceplate.
Version
Description
1.0 by Sumit Gargav
The block is used for running a timer of preset time during each hour of a day.The block uses the controller time as an input for date and time.The input pins H01, H02…., H24 are for running the timer in a particular hour.The out will be high for preset duration of the timer.The Timer can also be started from the faceplate. The buttons on the faceplate are for running the timer during each hour.Duration, Running current hour and Elapsed time of the timer is shown on the faceplate.
You must be logged in and have downloaded this app in order to post a review or rating. Login
Posted by
on
Apr 11, 2018 at 09:31 AM
Posted by
on
Apr 11, 2018 at 09:31 AM
Posted by
on
Jun 15, 2013 at 06:57 AM
Posted by
on
Jun 11, 2013 at 05:37 AM