Freelance 3D Macros - Version 1.1 (.zip)
App id
20194620
File extension
.zip
File name
232_Gauge_Macro-1_1-1.zip
Type
App
Version
1.1
File size
30 KB
Graphic macro for temperature and pressure value display in gauge format. Use related logic along with macro.
Follow the description file to use this macro in DigiVis.
Follow the description file to use this macro in DigiVis.
Version
Description
1.1 by Sumit Gargav
Graphic macro for temperature and pressure value display in gauge format. Use related logic along with macro.
Follow the description file to use this macro in DigiVis.
Follow the description file to use this macro in DigiVis.
Graphic macros for use with DigiVis. Includes basic components such as motors, pumps, valves, tanks, and pipes.
You must be logged in and have downloaded this app in order to post a review or rating. Login
by joytaderera Rank: 1465 on Sep 07, 2018 at 06:48 AM
Hello,
Thank you for the 3D application.
Im using the Demo version 10.3.9142 and i seem to be having problems with loading the macros.
Under the Software node, below, i inserted an operating system (D-OS) and then on the next level, Graphic Display (FGR)
By dlicking on the FGR , i used the 'Macro' option from the menu and then 'library functions' , then 'Load'
Load through browsing takes me to the 3D_Macros_revD.bol file. When i press "Open" for loading , Nothing loads
Am i doing something wrong?
Please would you assist. Thank you