Cannot delete from all structures
Inserted an from control structure into a different location inside control structure, which resulted in that the object itself received two control structure aspects and cannot be deleted. Neither the original object nor the inserted object can be deleted, not even with advanced -> delete from all structures.
Is there anyway I can delete the object?
Screenshot of how it looks like is attached
Answers
Unless you can delete the structure reference aspect (the aspect named "Control Structure") belonging to the wrong object I think you need to ask regional ABB to open a support case.
There are tools available that can remove any object without any questions asked. Obviously, they must be used with care.
Add new comment