"Freelance2000OPCServer.nn "can not be disabled, "Freelance2000OPCServer.nn" kann nicht deaktiviert werden
Error Code from Client:
IOPCGroupStateMgt::SetState Return Error Code=80010105
Voted best answer
Hello Klaus,
Could not figure out what issue you are getting at front side of application! As you are not using tunnel and OPC server clients are on same PC there is no issues of DCOM, using browse function you can see every item, Starting of OPC server works fine, from tracelog
“12/14/12 13:45:20
OPC group "Group_1" on OPC Server "Freelance2000OPCServer.50" can’t be disabled.
IOPCGroupStateMgt :: SetState Return Error code = 80010105 Invalid return code”
Seem issue with OPC group property setting either by client/server, However suggested to contact local ABB L3 support line people.
Answers
Hello Klaus,
could you give some more details like used Freelance version and operating system? Did you connect the client and server by DCOM or by a tunnel?
Is the OPC server running on its machine?
Hello,
we are using windows 7 Enterprise (64bit); Freelance Version 9.2 SP2.
OPC Server (Freelance) and OPC Client (NI DIAdem) are running on the same machine. We are not using the OPC-Tunnel.
By useing the Browse - funktion at the client I can see every Item; also starting the OPC server from the Client works o.k.
See Tracelog at the attached file:
by admin Rank: 46 on 12/14/2012 6:03:38 AM | Like (0) | Report
Edited by Admin: Thanks to google translator, added title with english language to get more responce from community.
cheers
Admin
Add new comment