Configuring the exchange of GOOSE messages over IEC61850 between REF615 and CI868
Help configure GOOSE messages between CI868 and REF615 using the PCM600 so that you can configure the PHIPTOC1 parameter in REF615 using CI868.
Answers
Hi.
The best and most comprehensive help should be available in the respective IEC 61850 engineering documentation:
- "AC 800M IEC 61850 Configuration for CI868":
- "615 series IEC 61850 Engineering Guide"
https://library.e.abb.com/public/b9752ab31e4343b183ef77e59b24c0d7/RE_615_61850e
ng_756475_ENn.pdf
Add new comment