problem with MCM800 vibration signals with AC 500 profibus
Good morning,
It seems that there is a problem with AC500 for the conversion of MCM Vibration signals to 4-20mADC using Profibus bus DP.
Please let us know if anyone of you have come across or heard anything like this.
I have attached few documents for your reference.
Thank you.
MCM800 document link
Answers
Hi
Can you please explain what kind of problem you are facing ????
1. Is Communication working on Profibus with AC500
2. you can configure in MCM.
3. Is there is Issue in Reading the Vibration ?
4. Readings not Matching with Field ?
you talked with ABB AC500 Supportline ???
Please send some screen Shots and Expalin your problem then may be we able to resolve issue
Regards
Source: AC500 MCM Communication
by admin Rank: 37 on 9/8/2014 1:06:16 AM | Like (0) | Report
Edited by Admin: Direct attachment of MCM800 document is removed as that document is not for public community.
by GustavA Rank: 71 on 9/8/2014 2:47:13 AM | Like (0) | Report
What is the issue? Communication? or what?
Add new comment