Freelance AI810 DTM - No Channel Updates on DTM Observe Window
When observing the DTM within Freelance 2016 SP1 RU1 the Channel values do not update on the DTM display window - Are ther any known issued regarding this?
Voted best answer
Yes, there is known issue with AI810, AO810 and DO820 in DTM version 6.0.1, which is shipped with the Freelance Software 2016SP1RU1.
A bugfix is currently in Test.
I'm not aware whether the DTM version shipped with F2016 (which was a 5.3.5022..) will still work with F2016SP1 but if you don't have the choice to wait for the fix you could try it out.
Add new comment