Create History Database Problem
Hi,Hope you are doing well!
I have installed the system in Automated mode with compliance of all prerequisites, installation and post installation up to the step : "Create History Database" in IM server, I used default value for all of the items in this wizard and the problem is the next button is still inactive after 2Days!.I will appreciate if anyone can help.
Answers
If on 64-bit Windows ensure that there are no "roaming NICs" (eg network cards with undefined DHCP addresses).
Disable all but primary client/server NIC and try creating the database again.
Dear Stefan
Thanks a lot but i am using the 32bit version of windows 2008 Enterprise and 800xA 5.1
Hi
Is the problem repeatable..
Anyhow it should not take that much time. With default values, it should take more than 1 hour.
I will recommend you cancel this somehow. Drop the database using Oracle Instance Wizard and try recreating one.
OR
You can send all files kept at %HS_LOG% for analysis.
Best Regards
Sunny Khatri
Dear Sunny Khatri
Hi,to tell you the truth it is a repeatable problem and i have tried it several times.
anyway, where can i find the HS_LOG file?
Best Regards.
Add new comment