Virtualization for version SV6.0
Good afternoon , we are going to upgrade the Control Builder A for Master from Aplication Builder 2.6/0 1999 , FucntionChartBuilder 4.6/0 1999, OnlineBuilder 2.6/0 1999, Windows NT 4.00.13811.2 to 1.4/1 , to Control Builder A 1.4/1 and we are thinking to install it into one of the connect node beside of that this connect node will be virtualized , Is there any restricction to dot that ?
Thanks for your support
Best Regards
Ricardo
Answers
No, it should work fine as long as prerequisites are fulfilled.
We are using Esxi 6.0 version , but same is not certified by ABB
We have make sure tehe Esxi 6.0 is certified with the Server hardware model selected.
as virtualization prodcut manager Esxi 6.0 will be approved in 800xa 6.1 release
Add new comment