800xA Alarm - Remove RTN, MBL, ABL is
How to disable these alarm state with state RTN ABL and MBL ?
I don't know recently it's started coming these alarms. It was not available before.
I want to get rid of these alarms as it is causing red / yellow circle in may places...
Answers
Have you tried acknowledging them?
What PLC emitted these alarms?
RTN (Normalized) and ABL (Auto Disabled) alarms are already in normal state, only they need acknowledgement to remove from the Alarm list.
MBL (Manually Blocked/Disabled) alarms are the ones which are disabled from the users. By default 800xA alarm list shows only 'Enabled' alarms. So it must be changed by someone to show even disabled alarms. Hence Disabled alarms appear irrespective of its active (ACT) or normal (RTN) state. Either you need to delete the disabled alarm or you have to enable it again and acknowledge the alarm once normalized.
Add new comment