Communication problem between pp882 and AC800M
Hi i am using a AC800M controller. I have installed Panel builder 800 v6 for PP882. I have downloaded the program to PP, but when i connect PP to controller it wont get connected as its showing communication error. I have used a ethernet cable for connecting PP and controller and i have set my controller ip as 172.16.15.23 and my PP ip as 172.16.15.23. Also i have used com port 3 of my controller to connect PP.
Answers
Hope this link Works:
AFAIK only port 1 and 2 can be used for Ethernet communication. Port 3 and 4 are serial communication ports.
For exchange of MMS without involving a router, the PP and AC 800M must share same subnet, but not IP.
Add new comment