Too many aspect
Dear all,
When I restore the back up of 800xA v3.1 into v 5.1 everything restore fine but during restore of Functional structure it Shown "Too many aspect" and import failed.
But I can open Control builder project not graphics.
Please help me What should I do?
Voted best answer
I suggest the problem could be due to the presence of more than one function structure aspect for the objects in the function structure.
Deleting the unused aspect could solve the problem.
Answers
You need to upgrade to 3.1 SP3 and pass the 3.1 SP3 backup through 5.0 SP2 (preferably RevE) before restoring it in 5.1.
At 5.0 SP2 Rev E, you should perform a Consistency Check before taking the backup into 5.1 and once in 5.1 you should perform a second Consistency Check to ensure all is well with the import.
Whenever you get a problem with import/restore - a logfile or screen capture of the restore/import problem would help us to understand what went wrong.
Don't hesitate to contact your regional ABB support center for help with the upgrading.
/Stefan
Add new comment