ABB Freelance IO editor
i want to assign my variables to the hardware S800 I/O what are the necesory/Precautions step i should perfrom before assigning them to the I/O cards
Answers
Hi,
Just use this associated two apps if you are using S800 I/O via gsd, everything is taken care to use s800 i/o with freelance controller over profibus.
Nevertheless there is nothing to be precautious as in freelance things are pretty simple. only you need to use variable datatype INT(Integer) for analog values to assign variable to S800I/O channels in I/O editor.
Btw I am curious why you have this is question ! nevermind.
Some more information you can find in this threads linked here with,
http://www402.abbext.com/How-scale-Analog-Input-Scale-Change-Block-q826887.aspx
http://www402.abbext.com/how-configure-DI-channel-FBD-CBF32013-blocks-needed-se
quence-q883383.aspx
Add new comment