How to impore PG2 graphic quality for large displays
We have just bought a bigger screen 42" and would like to convert some views for the new display but the objects seems to be blurred. The pixel size do increase with a bigger screen and same resolution but I did expect better sharpness.
We are using Pulp and paper PG2 graphics objects, for instance the valve objects does not look sharp in the edges and the green color make the object even worse.
Are there any settings I could make to improve the sharpness of the graphics objects?
Voted best answer
I have solved the problem. It's a setting for the RGS in General Tab --> Maximum image quality. Increase this to 100 and the image will improved.
Answers
Hello,
probably your problem depends on the graphic card, but it can also depend on wrong size of your PG2 display compared to the size the Workplace wants. To verify this:
If you are using 800xA 5.1, under Program Files\ABB Industrial IT\OperateIT\Process Portal A\demo you install demo displays with LoadNewGraphicsDemo.bat, if you don't already have installed it.
Under Functional Structure/Root/New Graphics Demo/Size Display, you find a display called SizeDisplay. Drag and drop to your operator workplace (or eg set SizeDisplay as startup display).
The displays you have should have the display size as SizeDisplay is indicating.
/Ronny
Add new comment