how to install DigiVis in windows 7? Is. windows 7 support DigiVis software??
For AC800F...configuration in need DigiVis software Installation. But in windows 7 DigiVis not get install. So i need a help to install DigiVis..
Answers
hi,
Seems version compatibility issue!
which freelance/digivis version you are trying to install and is it 32 or 64 bit W7 ?
Check this link below, table shared by linhan will answer/help to install digivis on w7.
http://www402.abbext.com/CBF-DigiVis-Freelance-9-1-64-bit-system-q14735.aspx
So if your OS is W7 32 bit, then supported version is Freelance V9.2 SP1 or SP1, lower version then this not supported. in that case you need to upgrade to higher compatible version.
Hope that helps.
Add new comment