Facing probleme in Control Net (Lan) Redundancy with PM-902F
Software /OS:- Freelance-2016 SP1 (Win-7 64 Bit SP-1)
Redundant PM-902F Controller
We are facing probleme with PM-902 F lan redundancy as:-
1. Configured on-board port of PC as primary lan and add-on port as a secondary lan.
2. When removing primary lan cable of engineering station; Process station is showing 'No Connection" while at the same time; able to ping controller with secondary lan cable of engineering station.
We have kept ID adresses like:-
On board LAN (PC):- 172.16.1.25 (Subnet Mask:- 255.255.240.0)
Add on Lan (PC):- 172.16.16.25 (Subnet Mask:- 255.255.240.0)
Primary CPU ETH-1:- 172.16.1.10 (Subnet Mask:- 255.255.240.0)
Primary CPU ETH-3:- 172.16.16.10 (255.255.240.0)
Primary CPU ETH-2:- redundancy link
Secondary CPU ETH-1:- 172.16.1.11 (Subnet Mask:- 255.255.240.0)
Secondary CPU ETH-3:- 172.16.16.11 (255.255.240.0)
Secondary CPU ETH-2:- redundancy link
Please let us know where we are going wrong and help us with expert suggestion/ comments.
Best Regards,
Rachit
Answers
May be the switchover time is the problem.
You can pretend a switchover time between 60s and 1s.
Standardtime is 45s.
Sorry but i have only a german installation.
Add new comment