Panel 800 vibration level
in Panel 800 technical information, it is emntioned Vibration is "A". Anyone can explain more about Panel 800 vibration resistive?
As I nknow vibration level of Automatioin devices are based on G like 2 G, 3G,..
What does mean "A"?
In compare with others?
Could client use it in vibrated panel?
Voted best answer
The PP871, PP874 and PP877 have DNV certfication.
The products have been tested according to that vibration test specification.
The specification for DNV certificates and their tests can be found on this
link:
We only have DNV class A in regards to vibration.
The panels have also been shock and vibration tested to comply with the following EN standards, 10G has been used in the tests.:
EN 60068-2-6:2008 Vibration, sinusoidal
EN 60068-2-27:2010 Shock, half-sine
EN 60068-2-64:2009 Vibration, broadband random
Answers
Yes, there is only defined that panel correspond to requests according DNV (mainly for marine applications) standards. I will try to ask my colleaguses (can take some time).
There is also available CP600 panels, where is data available in Operation instructions document:
I will try to get info regarding 800...
Add new comment