what is the Contoller that support the profile control ?
Greetings
could you advice me about the controller that support the profile control
regards
Voted best answer
Hello,
In freelance you can use TS - Time Scheduler function block for profiling. Up to 32 run times i.e time durations you can define in this FB. And there are many more supportive features makes profile control easy to use. Check details of function block TS at path blocks > analog > TS ( time scheduler) last block. check typical profile to be controlled in image below
Also profile may be run using controllers from RnC products, using PID.
Source:
Answers
Hi,
The R&C prdocuct line contains the C310 wich is a field mounted controller capable of Profile control.
Regards
Niki
Add new comment