Missing Device Types
I am using AC800M with 800xA, CI854A, LD800P, LD800HSE, AI845, AO845A and DO820. I would like to control an Emerson process technology with these modules (writing my thesis about ABB DCS systems and I need to control this technology). I have configured the basic system, and i would like to add some field devices, but i could not find the right object type files for all of them at Solution Bank.
These are the field devices i would like to use:
Rosemount 8800D Vortex (HART rev2.)
Rosemount 8800D Vortex (FF)
Fisher Fieldvue DVC 6010 SS (FF)
Rosemount 3144P temperature transmitter with a PT100 (FF)
I found some files, but i think they are not good for these devices, because for example when I try to assign the devices in Fieldbus Builder, the following error comes:
"The capabilities file information does not match with the information in the device. Contact your device vendor to get the right capabilities file. "
I found DTM files for 8800D Vortex at the webpage of Emerson Process Management, but they are setup files, install external DTMs and I do not know they are usefull or not.
Is there any way to make these field devices work properly with 800xa?
Answers
Hi ,
You have to use the correct Device Types downloaded from the ABB Solutions bank for making the Devices work with 800xA DCS System.
by Sumit Gargav
Contact to dic@in.abb.com
Add new comment