How to connect CHMI server with Client? (Want to add one Client)
How to connect CHMI server with Client? (Want to add one Client)??
1.When I connect the system one msg is pop-up....RPC Server is unavailable....
2.second problem is like.....when I connected the node...in client pc, system is showing but it's not going to healthy mode....???
Plz suggest the solution of it.
If you have any write-up for CHMI node connection procedure plz send.
Answers
1. RNRP Monitor must display client when viewed from server (or vice versa)
2. Incorrect firewall settings may prevent connection
3. Hosts files can prevent connection if incorrect
4. Workgroup must work properly
5. User accounts and passwords must be mirrored, including 800xA service account
6. Service account must be local administrator
Add new comment