Freelance on Profinet
Hi,
I need to communicate with Siemens 343-1 Advanced (6GK7 343-1GX31-0XE0) via Profinet using AC900F. Is there any way to do that? Telecontrol or Profinet/Profibus converter?
Regards
Voted best answer
Hi,
I would recommend a Profibus/Profinet converter or a Modbus TCP/Profinet converter.
If the 343-1 provides an suitable interface Modbus TCP instead of Profinet could be a solution.
Answers
Hi
You can use UDP send/receive blocks on both sides.
i am also trying to Comuunicate over MODBUS TCP IP with Siemens S7-300,1200 through Scalance X108 over Modbus TCP with ABB Freelance AC900F i am using this Architecture secondly do i need to to define any data or Holding Register in CBF Kindly help
Add new comment