CLS popup
I want to know in which scenario Applications are running with temporary licenses unable to communicate with CLS server occur?
Answers
One of the most common scenario is when the connectivity between the cls client (where the application is running) and cls server is not not successfull.
Hi
In your statement, there are two different scenarios of prompts :
- Applications are running with temporary licenses
- Unable to communicate with CLS server occur
Applications are running with temporary licenses: This pop up will appear if you are running 800xA applications, which allow temporary license to be granted, without valid license.
Unable to communicate with CLS server occur: This pop up will appear if communication between CLS Server and CLS Client is disrupted. Example : CLS Server restart.
Best Regards
Add new comment