Freelance 2013 faceplate problem
For my project with redundant AC800F I am using Freelance 2013
I pass steps succesfully about hardware and software and now building my own
user function blocks and their faceplates
About faceplates ı am getting crazy, as you can see from picture any faceplate that
ı use in my graphic display there are gaps in its left and right side
These gaps stays always if ı am use my own faceplate or use faceplate from library
How can ı remove these gaps.
Thanks for help.
Voted best answer
The answer is easy - You can't. Without asking any questions I can guess You are using 1920x1080 or other 16:9 ratio resolution on Your Operator Station. DigiVis was designed long time ago, when ratio of 4:3 was the standard and as that it's also the standard for DigiVis. When using other ratio resolutions DigiVis widens faceplates a bit to match the wider screen, leaving the added space empty. As such there is no way You can delete the gaps.
If You try to open DigiVis in 4:3 ratio resolution and open Your faceplate, there won't be any gaps, but if You're using newer screens, the gaps are unavoidable.
One more thing - if You want to test other resolution always close DigiVis before applying any changes and reopen it afterwards.
Hope it cleared some things a bit.
Regards,
Mike
Add new comment