reporting
Hi everyone,
Should I configure the datadirect to each user's account to reach report data?I can see the report with administrator but I can't see report with other account.
Answers
Hello,
Post Install manual:
Add-in tools for DataDirect and Information Management History Bulk
Configuration are added into Microsoft Excel on a user basis. These add-ins are
added by default for the Installing User. To use these applications as any other
user, the corresponding add-ins must be installed in Microsoft Excel for that
user. Refer to the section on History Setup in
Industrial IT, 800xA - Information
Management, Configuration (3BUF001092Rxxxx), or DataDirect - Excel Data
Access in Industrial IT, 800xA - Information Management, Operation
(3BUF001094Rxxxx)
Normally I double click on the xla file on the disk where the AddIn like Datadirect is located, in this case ABBDataDirect.xla under Program Files\ABB Industrial IT\InformIT\DataDirect\bin
/Ronny
Add new comment