Unable to delete an FF Test Subnet
We are running an 800xA 5.1/FP4 system with FF. Someone created a small test subnet with an LD800 HSE object, an H1 Link object and an H1 Schedule object.
We are unable to delete this HSE Subnet and recieve the following error message:
"Failed to lock object "name" of the ABB LD800HSE object. See FF management Aspect View for details."
If I open the FF Project and look at the ABB LD800HSE that is giving us the error, it is highlighted in red. Also, I am unable to reserve the node.
Answers
Sounds like a hook error (hook=object/aspect specific custom code that is triggered when an object is manipulated)
I see two possible outcomes:
1) Repair what is broken so that normal delete becomes possible
2) Use of special R&D tool which can delete objects without running any hooks
I believe you will have to ask for advise from some FF support expert - please contact your regional ABB support center or ABB sales representative.
Add new comment