data direct login
I try to enter user name & Password to login to the data direct but I receive the attached error message.
Answers
I am assuming that this is an upgrade to either a higher level of SV 5.1 or some version of SV 6+. Please see attachment for adding original users back into the system. Additionally, there is a full explanation of this issue in the manual, 3BUF001092-xxx, under the heading Creating Users. Be aware that for SV 6.0.3, the folder location of the "Data" folder has changed, noted in the attachment.
Regards,
Geof Ledin
Do you need ABBSql() and the Batch PDL related functions in DataDirect?
Or are you just planning to use the ABBGetOPCDA(), ABBGetOPCHDA() and ABBAERetrieval() functions?
The three later does not need any login, nor IM while the first require an IM, a license for EXCEL_DA and an appropriately configured user in the AdvaInform Display server user database.
Hello,
You have to add the AID user from "Userexapmles to data folder" this step is clearly written while doing post configuration for IM via configuration assistant.
Add new comment