CODESYS OPC SERVER
I would like to ask you about the CODESYS OPC SERVER.
I have in my laptop a standard license of Automation Builder and it includes the CODESYS OPC v2.3 and v3.5.
However I need to design and setup a scada system to another pc, so is it possible to download the CODESYS OPC SERVER (v2.3 and v3.5) from the official site of CODESYS in order to communicate the scada server with th plcs?
Is there any other preferable solution about the OPC SERVER (for the connectivity of scada system with AC500)?
Thanks in advance.
Voted best answer
Dear friend,
1.Go to this Link:
http://new.abb.com/plc/automationbuil...
2.click Automation Builder 2.0 Download. The AB2.0 setup file will download.Install that setup file.
In that, Click that Installer options and additional tools drop down arrow mark.
click that Install additional tools.
Answers
Dear friend,
CODESYS OPC v2.3 and v3.5 is available on Additional Tools .
you can easily download from abb website and install in your SCADA pc.
For your reference, Kindly view my screenshots.
Dear vigneshwaran92rce ,
thanks for your instant response.
I have already downloaded the Additional Tools, however there isn't the option of
OPC v3.5.
I can install only the OPC v2.3.
I notice in your images that you have the same version with me, so if you have any other idea I will appriciate that.
Add new comment