Which Block are used to know the Status of each I/o module and Controller in CBPlus 2.3
Hi guys,
I need information regarding the Controller Status and Each I/o module status which are the block are to used in the PS CBPlus Codesys2.3 to know the status of controller and Each I/o modules here in this case i have hotstandby system,with these tags i can link in digivis scada 500 ,if anyone has tried this kindly share backup.
As it is shown in system architecture, i have attached screenshot to better understanding.
Answers
You can use the Funtion block CS31_DIAG from the Library Diag_AC500_V10.lib
In this function block you can get the details like diagnosis data of all the CS31 software modules. For more details refer the help file of CS31_DIAG function block and of the CS31 library.
P S : This function block gives the diag info for software modules in the CS31 line, not the physical modules connected.
Add new comment