Engineering Board PU410 locked
I have a problem with one (PU410) units. We are not able to connect to one of them and I have tried to reset the unit many times without luck. The message I receive when trying to establish a connection to our MB300 network: Connecting to server "\\L2-SERVER". Please wait...
The Engineering Board is locked by: "". I try to use the lock/unlock button, but I don't have success.
Normally if it is used by one of my colleague it will say so and try to connect to another PU410 to gain access and that works as intented.
But I need to kill this connection in some way and had hoped by resetting the device it would have done so. There should also be an option to log on the RTA board config and kill the connection in that way, but I am not sure which task to kill if it is a task!
Answers
Google Translated into English Language
"Good evening,
The PU410 is a one of the engineering briefcases? or you are using a desktop computer?
Who are you trying to connect? (AC450, MP200.etc ..)
If you want to send me an email with the architecture of your system and what hardware and software versions you are using, I can try to help you.
any questions I am available."
Source:
Add new comment