Process Panel 800 freezes after a week
I have five PP865 Process Panel acquiring data via control network.
All of them always freezes after a random time between a week or a month of operation.
I can see that it has frozen because of the still clock on the screen.
It returns to activity after a power cycle.
The firmware revision is 4.0/2 B211.1.6. (se attached image).
What should I do?
Voted best answer
1) Check for firmware update
2) File a support case with regional ABB
Answers
What is the data source, AC800M? How many CPU's? How many CPU's you read from each panel?
For MMS driver I have ver. 5.06.01 - it is available trough Internet update.
Did you define in AC800M, CPU:
AE Max number of event subscribers = total number for each CPU (SCADA and panels)
Add new comment