How to config freelance for show 2 page display on 2 TV
Dear All
I need to show 2 Television and 2 page of 1 digivis what can I do . It can do not?
thank you for recommend
Arthit
Voted best answer
Hi,
You can't show two screen per display. But can I ask which twothings you want to show in one screen? In-case you want any graphic/systems display/message list in background and want to show trend as second screen can be possible via trend in faceplate. (check associated APP)
however you can have dual screen by default. Also now digivis supports quad-screen, just you need 4 display driver.
hope that helps.
Answers
Hmmm...
I read that question as a request to have 2 displays of a single DigiVis on 2 monitor screens. That would be the classic dual monitor operation.
Technically you need a graphics card that supports 2 monitors. We recommend a Matrox Millenium P690 or successor product. Just connect a second monitor to the DigiVis Station and then restart DigiVis. You can then switch between the monitors with your mouse and call up the displays seperately on your 2 monitors.
Don't forget that Dual Monitor is a licensed feature. You need to aquire a license to use it in production.
Add new comment