Compact HMI 800 V5.1 in Windows 7 64 Bit???
Will the compact HMI 800 V5.1 run on the following OS?
Windows 7 Professional SP1 32 Bit
Windows 7 Professional 64 Bit.
Voted best answer
Hi
From the Compact HMI 800 5.1 Revision B Release Notes:
Compact HMI 800 5.1 Revision B is a life cycle release and contains the following
updates:
-
Support for the 64 bit operating systems Windows 7 and Windows Server 2008 R2.- Support for Internet Explorer 9 has been added. Internet Explorer 8 and 9 are now both supported.
Regards,
Kumail
Add new comment