How do i get the OPC Server on an ABB PGP to work
I have an ABB Power Generation Portal version 4.1 with base license.
the OPC Component is installed but i cannot connect to it or browse it using an OPC client.
Could it be that the OPC Server is not activated.
thanks
Voted best answer
Hi, check base licences, if there is missing client, you will need extension according next info:
by uzohonic Rank: 3714 on 11/15/2013 12:33:05 AM | Like (0) | Report
hi find below a copy of the license file Certificate.
PGP 4.1 Base
Software under license:
Licensed options: 1 Server Configuration Standard Server, Primary 1 Local Client Yes Real Time Data Server Tag Capacity 5000 realtime tags Harmony Connect Yes OPC Server Functionality No DDE Connection Support No ODBC Server Support No P13 Connect No History Logs 2500 History Logs API Support No Simulation Support No Calculation Engines No Local WEB Server Support (10 clients) No Freelance, AC800F & AC800M Connect No Remote Clients Support No Remote Clients Reserved-NT Must be 00 Harmony/INFI Yes Reserved-DR Must be zero OPC Client No ODBC Client No MODBUS / MODBUS TCP (Master) No SPABUS No IEC 870-5-101 (Master & Slave) No IEC 870-5-104 (Master & Slave) No
by uzohonic Rank: 3714 on 11/15/2013 12:39:42 AM | Like (0) | Report
Software under license:
Licensed options: 1 Server Configuration Standard Server, Primary 1 Local Client Yes Real Time Data Server Tag Capacity 5000 realtime tags Harmony Connect Yes
OPC Server Functionality No
DDE Connection Support No
ODBC Server Support No
P13 Connect No
History Logs 2500
History Logs API Support No
Simulation Support No
Calculation Engines No
Local WEB Server Support No
Freelance, AC800F & AC800M Connect No Remote Clients Support No
Remote Clients Reserved-NT Must be 00 Harmony/INFI Yes
Reserved-DR Must be zero OPC Client No ODBC Client No
MODBUS / MODBUS TCP (Master) No
SPABUS No
IEC 870-5-101 (Master & Slave) No
IEC 870-5-104 (Master & Slave) No
Add new comment