Backlight savings ProcesPanel pp845
If have a procespanel type pp845 on which I cannot find/configure the settings fot the backlight saving (= screensaver). At this momment the panel is lit contineus.
Where can I configure the backlight settings.
(PS, I find already the option : alram settings > backlight > Timer. But changing this parameter does not do anything?)
Sjoerd
Voted best answer
Please select the Terminal Options in the Setup menu:
Change the Screen save time from 0 to any other value.
Screen save time
The time in minutes after the last event on the display when it will switch off. The default setting is 0 which means that the display never switches off. This function optimizes the service-life of the display.
Source: On line help (F1) for the Panel Builder 800 version 5.1
Answers
Setup\Terminal Options\Screen save time
Ok Thanks, I just didn't see the option, read over it :(
Add new comment