HMI CP607 data to be seen on webpage.
Hi everyone,
I have this project in which i have dispalyed the values of level transmitters on the hmi and now i have to display the same on the webpage. The feature is available in CP 607 higher version,and also how to display the values on tablet?
I'm using PLC PM554 TP-ETH and the ip address is 192
.168.0.10 and the ip address of the HMI is 192.168.0.20
Please suggest any demo link for the same if available.
Thank you.
Answers
Greetings
As far as I know, CP600-eco series panels do not suppot WebServer action.
You have to use CP6x0-WEB operator panels, or you can use AC500 PLCs,PM554-ETH CPU has built-in WebServer support.
You have to create a webpage and related it with variables, and then user has to open webbrowser with an address: http://192.168.0.10:8080 Thats all.
Hope this helps you.
Add new comment