Freelance 2016 SP1 RU01 AC700 error 3000 0203
Hello,
I have made an uppgrade from 9.2 to 2017. The 800-controller works fine
and 5 AC700 also works fine.
One AC700 restarts very often and give the errorcode 3000 0203, CPU unaligned.
I have run the testprogram and got an OK.
No other errors from the CPU.
Anyone an idea?
Best regards.
Tore Wassén
Answers
Dear Tore,
Get connect with your local supportline,
This is related to programming/Application, seems some structured data type are used, And while using in it in some functions both structure data type dosen't match. means in one of the structure datatype some of the element is missing.
Requested to get connect with supportline and ge this fix or resolved.
Hope and wish rest all is well at your end.
Cheers.
Add new comment