Removal of VB aspects in 800xA 6.0
Hello,
I use some Extension libraries in 800xA 6.0.
The libraries for Version 800xA 6.0 has no VB aspects. It contains only PG2.
However, as VB aspects were present in the Previous versions (5.1 System), when an upgrade is done to 800xA 6.0, the object type structure has both VB & Pg2.
How to remove these VB aspects coming from old Project backup (i.e 5.1 System)
Any tool exists to do this?
Please guide.
Answers
You have to speak to the vendor of the library which can be yourself, a partner, a delivery project, third party or ABB.
In 6.0.0 the VB aspects will be imported (but VB6 is not supported...)
In subsequent versions (6.0.1 and onwards) VB6 aspects will automatically be "nulled" when imported. With nulled I mean, aspect will be visible in Plant Explorer, but not operational.
Personally, I would strive for having VB6 and PG2 in separate Extension Libraries, and on 6.0 just delete the VB6 extension library off the system to keep only PG2.
by SG Rank: 50 on 5/25/2017 11:47:17 PM | Like (0) | Report
I tried to unregister & delete the system extensions from Admin structure.
But this does not work in all systems
Add new comment