Impossible to create signal on Online Builder
Hello, I have a problem.
I can't create DOC signal with TRDBS.
And wenn I connect with MDB DOCxxx, the signal don't exist.
What can I do?
Answers
TRDBS failure can have two possible reasons:
1. Wrong instance ID, edit file and replace instance ID with *.
2. Database dimensioning, not enough room for new DO:s, redimension database.
Why dont you create it on-line, using "CRDB DOC"? If that doesnt help, youre facing problem no 2 above!
How you generated the DB Source File ?
Source file to be generated only with required DOC.
Translation should work !..
Add new comment