PCM600 event viever not visible
Hello,
I use PCM600 v2.8 and REF/REU615 relays. I like to read event from relays and there should be two possibilities to start event viever:
But for some reason Event viever selection is totally missing. Every other tools are visible but not event viever.
Answers
Is it possible that you have hidden the Event Viewer with 'Customized Menus' -functionality? Please disable the functionality from the main menu View > Disable Customized Menus and try again.
If that didn't help, could you:
- Tell me the used REF/REU615 Connectivity Package versions. You can find these versions from Help > About PCM600
- Attach a screenshot where I can see the 615 IED selected in the Plant Structure and the Tools menu opened for it.
Another reason for not seeing Event Viewer might be that the support for Event Viewer tool was introduced for 615 series in the release 4.0. So if your devices are 3.0 or older then they don't support Event Viewer.
Add new comment