Workplace crashes when editing a Valvecon Faceplate to callup (new icon) another object.
800xA System version 5.0 for Advant Master.
When adding a DO icon in a Valvecon Faceplate, sometimes the Engineering Workplace freezes or Crash. (one fail in every 3 or 4 attempts).
In Object Type Structure /... Object DO, aspect: Faceplate, we add an empty “Graphic Display PG2” as a button.
In the Valve objects (type Valvecon) for each tag we did an Override in the Faceplate aspect.
Configuring the (added) button to call up another object (in this case a DO Faceplate) sometimes the Engineering Workstation crash or freezes
eg.: Changing the faceplate for a Valve H35025, set the Aspect Link to a DO object HVK35025, (View: Extended).
1. In ControlStructure/Object H35025, aspect Faceplate – Click Override.
(Sometimes after this the engineering workplace freezes or close, and we have to do once again)
2. Calling up the Config View of the object H35025, and point up the Object to be called (HVK35025)
(Sometimes after this the engineering workplace freezes or close, and we have to do once again)
The Errors we got are like:..
11/01/2017 14:07:36:
PID: 844 (0x34c), TID: 3984 (0xf90)
Fault Reason:
-------------
AfwWorkplaceApplication.exe caused an EXCEPTION_ACCESS_VIOLATION in module ntdll.dll at 001B:7C9113A0, RtlDeleteCriticalSection()+0070 byte(s)
...
or...
12/01/2017 09:28:35:
PID: 3544 (0xdd8), TID: 3108 (0xc24)
Fault Reason:
-------------
AfwWorkplaceApplication.exe caused an EXCEPTION_INVALID_HANDLE in module ntdll.dll at 001B:7C96478E, RtlRaiseStatus()+0038 byte(s)
The procedure and Errors we got are in the attached files.
Can anyone explain what is happening?
Answers
This question has not yet been answered.
by Stefan Stromqvist
Hello Ayrton!
Probably a bug, I will try to get a developer to look at the exception text, but I fear little or nothing will be made for 5.0 (hey, even 5.1 is nearing its end of active product life phase and efforts are moved onto 6.).
Add new comment