Freelance HART possibility
Hi,
I´m evaluating the possibility to use Freelance on a project. One specific requiremement is to connect a Pepperl+Fuchs Universal IO (LB7004A, LB7104A) with Hart modules to Freelance. And also I need to have acces to DTM displays of connected HART field instruments in Freelance Engineering. Does anyone have such experience?
I´m evaluating the possibility to use Freelance on a project. One specific requiremement is to connect a Pepperl+Fuchs Universal IO (LB7004A, LB7104A) with Hart modules to Freelance. And also I need to have acces to DTM displays of connected HART field instruments in Freelance Engineering. Does anyone have such experience?
Answers
Freelance generally supports FDT/DTM Technology and also nested DTMs which would be the case of a HART DTM below a remote I/O DTM.
Particularily P+F Universal I/O I don't know. It was not compatibility tested as can be seen from the latest "Freelance Integrated PROFIBUS Devices" datasheet.
Maybe P+F has some knowledge about their I/O being used together with Freelance.
Add new comment