Microsoft patches centralized deployment for 800xA
With a system size of 60-70 nodes it is time consuming to run "ABB qualified security update installer" on each node. How can we deploy the patches centrally
without having to go to the node and without having to click few buttons.
Voted best answer
There are several ways you can do this ( using either WSUS or ePO server). Some guidelines are given in our documentation which can help you in configuring them.
Refer to the section "Management of System Updates" in 800xA Network Configuration manual for more information on this (3BSE034463-510).
Answers
You need to define a group policy for WSUS that allows domain members to update from a server inside your control system and then enable Automatic Updates on each domain computer.
Use your favourite search engine to read about Windows Software Update Service and how to configure it. Start here ....
http://technet.microsoft.com/en-us/library/cc720539(v=ws.10).aspx
Add new comment