question about VNC Client as PG2 Primitive (1.0)
is the app for version 5.x ?
are you planning it to change for version 6.x
Answers
This App is written and tested with 5.1.
I would test and (if needed) fix it for 6.0, if I could have access to a 6.0 Test System. On my plant we are still on 5.1, and this will also be for a while.
I have already asked for a 6.0 test version. My local ABB dealer will take full license money for such a system!
If You like You can test it with 6.0, and share your experiences.
I've tested it on version 6.0 but its not working.
The DLL is not working on Server 2012, and the directorie is not available in version 6.
C:\Program Files (x86)\ABB 800xA\Base\bin\GraphicPrimitives\pg2vncviewer.dll.
Add new comment