New template to bulk the AI_TR parameters in Freelance 2013 BDM
Hello,
is it possible to add a new template to the Freelance bulk-data-manager?
I want to bulk the parameter of the AI_TR Funktion-Block but there is no template for the AI_TR.
Voted best answer
I understood your problem,in present version there is no template for AI_TR function block so it is not possible to bulk the parameters of the AI_TR FB's. Whichever function blocks are available in templates only those function blocks parameters you can bulk.
Answers
Hi,
I understood that you want to multiply/bulk AI_TR Function block using BDM in Freelance 2013.
Yes, you can multiply/bulk AI_TR Function block using BDM in Freelance 2013 with existing templates, no need to add any new templates for AI_TR function block.
Procedure:
1. Export to BDM from P-tree, save & close CBF, select Start session -> Select Export
2. Select Program name which contains AI_TR function block -> select export
3. Excel template will get open, copy full Row (path,tag,variables) and paste in next Row and rename the tags and variables.(need to rename all tags & variables)
4. Save & close Excel and select import from BDM tool.
Please correct me if my understood is wrong.
Add new comment