what does it mean by PARAMETER ERROR in CI840 SLAVE ?
Attempting to configure a new harrdware with ACS800(redundant), which include a RLM unit and a profibus slave unit with CI840A.
Project is downloaded to the PLC,but in commisioning mode error shows as "PARAMETER ERROR IN SLAVE".
Answers
Have a look on the placed modules.
Are the modules in the project the same as in the cabinet placed?
Also have a look on the position of analogue modules. They must be adapted.
Add new comment