How can i add a printer on 800xA v4.0.
How can i add a printer on 800xA v4.0. I had a printer installed in a control room which was accessed from work station and 4 operators. It got unhealthy now i have installed a new printer. Where do i add the printer ?? The workstation ?? How to configure it ?
Voted best answer
This is a pure Microsoft Windows question - how to add a printer.
Please search among the standard Microsoft documentation for Windows XP / 2003 Server.
Once the printer has been added and visible in Windows you can use it in 800xA to print.
There are several options; use one computer as printer server or if printer is networked all computers can connect to it directly without having to pass print job via a queue.
/Stefan
Add new comment